Please share the procedure to commit new changes to Kernel in Yocto environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please share the procedure to commit new changes to Kernel in Yocto environment

1,543 Views
pranav_s
Contributor II

Hi,

I want to include few drivers in Kernel, please let me know the procedure to commit the changes in Yocto environment.

I could some patching mechanism is to be used but no clear understanding. We are working on Ls2088a based project.

Please guide.

Regards,

Pranav

Labels (1)
0 Kudos
Reply
1 Reply

1,476 Views
Pavel
NXP Employee
NXP Employee

There is information about adding driver in Yocto in internet.

See the following pages:

https://lists.yoctoproject.org/pipermail/yocto/2017-October/038459.html

 

https://forum.mangoh.io/t/add-driver-to-yocto/1204

 

https://forum.legato.io/t/add-a-kernel-driver-in-the-linux-yocto-3-4-recipe/1992

 

https://lists.ubuntu.com/archives/kernel-team/2014-August/047307.html

 

NXP offers non Yocto Linux BSP for the LS2088a - LSDK.

See the following page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply