Pin Mux tool for QorIQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Mux tool for QorIQ

4,622 Views
deepaknaiknavar
Contributor II

Does the QorIQ family have any Pin Mux tool that allows pin configuration of LS1021A processor?

I have searched but could not find it for QorIQ family.

If no, what would be the best possible way to go ahead. Thanks!!

Labels (1)
7 Replies

4,122 Views
addiyi
NXP Employee
NXP Employee

From the QCVS project wizard, you should select Pin Muxing Configuration, like below:

pastedImage_0.png

After that, you have to select the PinMux component:

pastedImage_1.png

Adrian

4,122 Views
deepaknaiknavar
Contributor II

Thats Great Help Adrian !!

Finally..the problem was because I do not have this component in the list :smileysad:

0 Kudos
Reply

4,122 Views
addiyi
NXP Employee
NXP Employee

If you select QCVS to be installed from the install wizard you should see something as below:

pastedImage_0.png

If don't see the QorIQ Configuration Project, go to Help > Install New Software and use ARMv7 Main Updater Site to install QCVS

pastedImage_2.png

Make sure during installation now ccs.exe or cdde.exe are present in Task Manager.

Adrian

0 Kudos
Reply

4,122 Views
deepaknaiknavar
Contributor II

Thanks Adrian !!

I have reached untill here. Here, i see Pin Multiplexing option but it does not have complete pins.

Is it correct?

pastedImage_2.png

0 Kudos
Reply

4,122 Views
addiyi
NXP Employee
NXP Employee

Please refer to www.nxp.com/qcvs. QCVS provides Pin Muxing Configuration tool for LS devices.

Adrian

4,122 Views
deepaknaiknavar
Contributor II

Hi Adrian !

I have installed codewarrior for arm 7 (QorIQ) Ver 10.0.8.

But i cannot find QCVS option. Is there any help to access QCVS pin mapping tool?

0 Kudos
Reply

4,122 Views
deepaknaiknavar
Contributor II

Thanks a lot !! It looks this will solve the Problem..

0 Kudos
Reply