PMU IRQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMU IRQ

4,386件の閲覧回数
nitesh-einfochips
Contributor II

I need to implement generation of an IRQ on overflow of a counter on 1046a . ARMv8 manual recommends using PPI 23 for this IRQ, but allows for board designers to use a different input. I wasn't able to find an explicit mention of the wiring of the PMUIRQ in LS1046A reference manual. Is there a specific  IRQ number  which I should be using when there is a counter overflow?

@igorpadykov @yipingwang 

0 件の賞賛
返信
7 返答(返信)

4,332件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check the table 5-1

Below information for PMU IRQ line is mentioned.

138 A72 core 0 PMU IRQ

139 A72 core 1 PMU IRQ

127 A72 core 2 PMU IRQ

129 A72 core 3 PMU IRQ

0 件の賞賛
返信

4,320件の閲覧回数
nitesh-einfochips
Contributor II
Do you have a sample example of how I can configure PMU interrupt when there is an overflow? @yipingwang
0 件の賞賛
返信

4,319件の閲覧回数
nitesh-einfochips
Contributor II

@yipingwang @Yuri I am looking into reference manual, and I can see I have to enable following regsiters
Select counter PMSELR_EL0, Select Event type PMXEVTYPER_EL0, setting interrupt PMINTENSET_EL1, start counter PMCNTENSET_EL0, write value to event counter PMXEVCNTR_EL0. I can see overflow getting generated by checking PMOVSCLR_EL0 register but I don't see interrupt getting generated. I am working on armv8.

 

タグ(1)
0 件の賞賛
返信

4,290件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

What is the value of PMCR_EL0 ?

0 件の賞賛
返信

4,283件の閲覧回数
nitesh-einfochips
Contributor II

@yipingwang Thanks for the prompt response. The PMCR_EL0 value when read before writing is Default Value) 0x41023000 after enabling PMU the value is 0x41023001. I am writing 0x01 to enable PMU.

0 件の賞賛
返信

4,235件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

As you explained, your setting looks fine to generate the PMU interrupt. Can you share the values of all registers you have set as well. Meanwhile we will try to replicate the same at our end.

0 件の賞賛
返信

4,321件の閲覧回数
nitesh-einfochips
Contributor II

Do you have a sample example of how I can configure PMU interrupt when there is an overflow?

0 件の賞賛
返信