PCIe link downgrade issue with ls1021a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe link downgrade issue with ls1021a

4,525件の閲覧回数
Anonymous
適用対象外

Running pci enum command in u-boot detects the gen3 device as gen1.

=> pci enum
PCIe0: pcie@3400000 Root Complex: x1 gen1
PCIe1: pcie@3500000 Root Complex: no link

0 件の賞賛
返信
9 返答(返信)

4,413件の閲覧回数
Anonymous
適用対象外

Is there any update on this from the development team ?

0 件の賞賛
返信

4,518件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Which version LSDK are your using?

Would you please provide your whole u-boot console log?

0 件の賞賛
返信

4,516件の閲覧回数
Anonymous
適用対象外

U-Boot SPL 2019.10+fsl+gde20a4439e (Apr 18 2022 - 12:53:00 +0000)
Trying to boot from MMC1


U-Boot 2019.10+fsl+gde20a4439e (Apr 18 2022 - 12:53:00 +0000)

CPU: Freescale LayerScape LS1021E, Version: 2.0, (0x87081120)
Clock Configuration:
CPU0(ARMV7):1200 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000c 00000000 00000000 00000000
00000010: 70000000 00007900 60040a00 21046000
00000020: 00000000 00000000 00000000 18000000
00000030: 00000000 841b7340 00000000 00000000
Model: LS1021A TWR Board
Board: LS1021ATWR
CPLD: V3.3
PCBA: V2.0
VBank: 0
DRAM: 1 GiB
Using SERDES1 Protocol: 112 (0x70)
si5341_clock_init: Cannot find udev for a bus 1
Flash: 128 MiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
Net: eth0: ethernet@2d10000 [PRIME], eth1: ethernet@2d50000, eth2: ethernet@2d90000
Hit any key to stop autoboot: 0
=> pci enum
PCIe0: pcie@3400000 Root Complex: x1 gen1
PCIe1: pcie@3500000 Root Complex: no link

0 件の賞賛
返信

4,514件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Do you use u-boot from NXP LSDK? Which version?

0 件の賞賛
返信

4,512件の閲覧回数
Anonymous
適用対象外

20.04

0 件の賞賛
返信

4,498件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following feature in LS1021ARM, PCIe gen 3 is not supported.

yipingwang_0-1650362157693.png

 

0 件の賞賛
返信

4,495件の閲覧回数
Anonymous
適用対象外

I understand gen3 is not supported. But why is it getting detected as gen1. gen2 is supported right ?

0 件の賞賛
返信

4,456件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

RCW[SRDS_DIV_PEX] is configure as "01".

0x Can train up to a max rate of 5 G

This is defect of LS1021ATWR u-boot, I will report it to the LSDK development team.

0 件の賞賛
返信

4,409件の閲覧回数
Anonymous
適用対象外

Is there any update on this issue from the development team ?

0 件の賞賛
返信