Of course, the PC specification is very high.
you think it's because of the LS1012A specification?
I had that thought at first, but I actually measured CPU utilization and it wasn't high..only 10~15%?
the system is LS1012A + WCN6856 (WIFI6 card) + yocto 5.15.5 + atk11 driver 5.17.1 + hostap 2.11
1. I ported 5.17 atk11 driver to yocto 5.15.5 kernel, because atk11 driver 5.15.5 show an error about MSI vector.. and I couldn't fixed it...so, I ported and it worked...
but...this could be the reason of limitation.
so...I am waiting the higher kernel version come out.
and NXP told me that the 6.1 version will be release in 2023..
I am just waiting for that time to come fast.