您好!
请问QorQ系列的P1010能否同时支持3个千兆以太网,1个PCIE, 1个SATA同时使用?还有,serdes使用的复用关系是怎么样的?
盼复,多谢。
Solved! Go to Solution.
Yes.
The P1010 SerDes could be configured as PCIe + 3xSGMII + 2xSATA (cfg_io_ports[0:1]=0b10).
Please refer to the P1010 QorIQ Integrated Processor Reference Manual, Table 4-14. SerDes I/O port and protocol selection.
> If so , how can the serdes reused in such domain?
The question is not clear - please elaborate.
Please provide English wording of the request.
Hi Sir:
My question is ,do the P1010 or LS1021 run the GMAC*3 and PCIe/SATA at the same time ? How about the vedio serdes to use in hardware?
Thanks !
> GMAC
SGMII or RGMII?
> PCIe/SATA
PCIe or SATA?
> vedio serdes
Sorry, what do you mean?
3*SGMII+PCIe+SATA , I see that the p1010 just has 6 lane to share with peripheral to run , can they work together?
If so , how can the serdes reused in such domain?
Yes.
The P1010 SerDes could be configured as PCIe + 3xSGMII + 2xSATA (cfg_io_ports[0:1]=0b10).
Please refer to the P1010 QorIQ Integrated Processor Reference Manual, Table 4-14. SerDes I/O port and protocol selection.
> If so , how can the serdes reused in such domain?
The question is not clear - please elaborate.
Hi Ufedor:
Thanks for your response , your reply solved my problem perfectly,thanks!
By the way ,could you have the qemu resource packages for P1010? thanks!
Please note that it is inconvenient to combine logically unconnected issues into a single thread.
Please create new question for your last request.
ok,thanks!