P1010/LS1021 lane 复用问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010/LS1021 lane 复用问题

Jump to solution
2,765 Views
bratzhang
Contributor II

您好!

     请问QorQ系列的P1010能否同时支持3个千兆以太网,1个PCIE, 1个SATA同时使用?还有,serdes使用的复用关系是怎么样的?

     盼复,多谢。

Labels (1)
0 Kudos
Reply
1 Solution
2,337 Views
ufedor
NXP Employee
NXP Employee

Yes.

The P1010 SerDes could be configured as PCIe + 3xSGMII + 2xSATA (cfg_io_ports[0:1]=0b10).

Please refer to the P1010 QorIQ Integrated Processor Reference Manual, Table 4-14. SerDes I/O port and protocol selection.

> If so , how can the serdes reused in such domain?

The question is not clear - please elaborate.

View solution in original post

0 Kudos
Reply
8 Replies
2,337 Views
ufedor
NXP Employee
NXP Employee

Please provide English wording of the request.

0 Kudos
Reply
2,337 Views
bratzhang
Contributor II

Hi Sir:

     My question is ,do  the P1010 or LS1021 run the GMAC*3 and PCIe/SATA at the same time ? How about the vedio serdes to use in hardware?

    Thanks !

0 Kudos
Reply
2,337 Views
ufedor
NXP Employee
NXP Employee

> GMAC

SGMII or RGMII?

> PCIe/SATA

PCIe or SATA?

> vedio serdes

Sorry, what do you mean?

0 Kudos
Reply
2,337 Views
bratzhang
Contributor II

3*SGMII+PCIe+SATA , I see that the p1010 just has 6 lane to share with peripheral to run , can they work together?

If so , how can the serdes reused in such domain?

0 Kudos
Reply
2,338 Views
ufedor
NXP Employee
NXP Employee

Yes.

The P1010 SerDes could be configured as PCIe + 3xSGMII + 2xSATA (cfg_io_ports[0:1]=0b10).

Please refer to the P1010 QorIQ Integrated Processor Reference Manual, Table 4-14. SerDes I/O port and protocol selection.

> If so , how can the serdes reused in such domain?

The question is not clear - please elaborate.

0 Kudos
Reply
2,337 Views
bratzhang
Contributor II

Hi Ufedor:

      Thanks for your response , your reply solved my problem perfectly,thanks!

     By the way ,could you have the qemu resource packages for P1010? thanks!

0 Kudos
Reply
2,337 Views
ufedor
NXP Employee
NXP Employee

Please note that it is inconvenient to combine logically unconnected issues into a single thread.

Please create new question for your last request.

0 Kudos
Reply
2,337 Views
bratzhang
Contributor II

ok,thanks!

0 Kudos
Reply