Off-Chip Trace LS1012A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Off-Chip Trace LS1012A

1,839 Views
guillaume17
Contributor I

Hi,

 

I'm looking for information or documents that tell me how to use the trace feature on LS1012A.

 

I saw that there was an Embedded Trace Macrocell (ETM).

 

I would like in my case to make code coverage. However, I can not find the port to use and the pins.

 

Is it possible to recover the traces with for example the LAUTERBACH Off-Chip Trace Solution probe ?
Is the trace port available and if so where can I find the pins?

 

Thanks for your help

 

Cordially

Labels (1)
0 Kudos
Reply
1 Reply

1,704 Views
ufedor
NXP Employee
NXP Employee

NXP CodeWarrior ARMv8 complex contains Tracing and Analysis Tool:

https://www.nxp.com/docs/en/user-guide/CWARMv8TAUG.pdf

> I can not find the port to use and the pins.

JTAG test/debug interface port is used.

> Is it possible to recover the traces with for example the LAUTERBACH Off-Chip Trace Solution probe ?

Please address this request to the Lauterbach directly.