Network Gbit Performance on TWR-LS1021A - high CPU utilization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Network Gbit Performance on TWR-LS1021A - high CPU utilization

ソリューションへジャンプ
2,416件の閲覧回数
reinhardtartler
Contributor I

Using a TWR-LS1021A board with SDK v1.8 (Linux 3.12.370rt51)

I've configured eth0 following the recommendations from Test Procedure

root@ls1021atwr:~# ethtool -C eth0 rx-frames 22

root@ls1021atwr:~# ethtool -C eth0 tx-frames 22

root@ls1021atwr:~# ethtool -C eth0 rx-usecs 32

root@ls1021atwr:~# ethtool -C eth0 tx-usecs 32

root@ls1021atwr:~# ethtool -K eth0 gro on gso on sg on

root@ls1021atwr:~# netperf -H 10.0.0.20 -l 10  -T 1 -c 100 -C 100 -n2 -t TCP_SENDFILE -v 2 -- -C

TCP SENDFILE TEST from 0.0.0.0 () port 0 AF_INET to 10.0.0.20 () port 0 AF_INET : cpu bind

Recv   Send    Send                          Utilization       Service Demand

Socket Socket  Message  Elapsed              Send     Recv     Send    Recv

Size   Size    Size     Time     Throughput  local    remote   local   remote

bytes  bytes   bytes    secs.    10^6bits/s  % S      % S      us/KB   us/KB

87380  16384  16384    10.03       886.20   76.23    18.60    14.094  3.439 

Alignment      Offset         Bytes    Bytes       Sends   Bytes    Recvs

Local  Remote  Local  Remote  Xfered   Per                 Per

Send   Recv    Send   Recv             Send (avg)          Recv (avg)

    8       8      0       0 1.111e+09  16384.00     67799   23129.53  48026

Maximum

Segment

Size (bytes)

  1448

In this setup, the other side is a Core2Duo x86 laptop @2.9 Ghz.

Using strace, I can confirm that netperf is indeed using the sendfile64 syscall:

root@ls1021atwr:~# grep -c sendfile64 netperf.strace

36850

The achieved bandwidth is less than we hoped, and the CPU utilization is unacceptably high. This is already after:

Why is the CPU utilization still so extremely high, and what can be done to improve this further?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Reinhard Tartler,

For ls1021atwr CPU Rev 1.0 board, when the frame size is 16384 bytes, the throughput data is about 850Mbps, this test result looks normal.

Would you please let me know your expected performance data?

If you are just in the evaluation stage, I suggest you choose ls1021atwr CPU Rev 2.0 board and "Linux SDK for LS1021A v0.4", you will get much better Network performance and lower CPU utilization.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,148件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Reinhard Tartler,

For ls1021atwr CPU Rev 1.0 board, when the frame size is 16384 bytes, the throughput data is about 850Mbps, this test result looks normal.

Would you please let me know your expected performance data?

If you are just in the evaluation stage, I suggest you choose ls1021atwr CPU Rev 2.0 board and "Linux SDK for LS1021A v0.4", you will get much better Network performance and lower CPU utilization.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信