NFS does not connect LS1046ARDB LSDK 1909

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFS does not connect LS1046ARDB LSDK 1909

1,916 Views
itzik_sherf
Contributor I

Trying to enable a boot from NFS process.

  • Standard Yocto build based on instructions, full network image.
  • The LS1046ARDB board is in its initial state, no changes in QFLASH or in U-boot configuration.
  • Booting the kernel from a boot partition on /dev/sda1 (SSD drive).
  • The bootargs are: ttyS0,115200 root=/dev/nfs nfsroot=10.0.0.15:/var/nfsshare rw ip=dhcp
  • The boot script is: bootnfs=scsi reset; ext4load scsi 0:1 a0000000 /boot/fitImage.bin; bootm a0000000:kernel@1 - a0000000:fdt@freescale_fsl-ls1046a-rdb-sdk.dtb
  • The NFS server works good, tried on CentOS and Ubuntu servers, fully accessible.
  • DHCP request succeeds, and it shows the right "rootserver":
    Sending DHCP requests ..
    [ 9.123360] IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready
    [ 10.738900] ., OK
    [ 10.764834] IP-Config: Got DHCP answer from 10.0.0.138, my address is 10.0.0.7
    [ 10.772062] IP-Config: Complete:
    [ 10.775288] device=eth2, hwaddr=00:04:9f:06:50:be, ipaddr=10.0.0.7, mask=255.255.255.0, gw=10.0.0.138
    [ 10.784941] host=10.0.0.7, domain=Home, nis-domain=(none)
    [ 10.790776] bootserver=0.0.0.0, rootserver=10.0.0.15, rootpath=
    [ 10.790778] nameserver0=10.0.0.138
  • After it is stuck for a while, it fails on Kernel panic:
    [ 208.354955] VFS: Unable to mount root fs via NFS, trying floppy.
    [ 208.361229] VFS: Cannot open root device "nfs" or unknown-block(2,0): error -6
    [ 208.368464] Please append a correct "root=" boot option; here are the available partitions:
    [ 208.376821] 0100 4096 ram0
    [ 208.376822] (driver?)
    ...
    [ 208.462581] (driver?)
    [ 208.468765] 010f 4096 ram15
    [ 208.468766] (driver?)
    [ 208.474961] 1f00 524288 mtdblock0
    [ 208.474962] (driver?)
    [ 208.481492] 1f01 65536 mtdblock1
    [ 208.481493] (driver?)
    [ 208.488031] 1f02 65536 mtdblock2
    [ 208.488032] (driver?)
    [ 208.494562] 0800 117220824 sda
    [ 208.494563] driver: sd
    [ 208.500667] 0801 5242880 sda1 9fb1f8e1-01
    [ 208.500668]
    [ 208.507034] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
    [ 208.515295] CPU: 2 PID: 1 Comm: swapper/0 Tainted: G W 5.4.3+gf811858 #1
    [ 208.523294] Hardware name: LS1046A RDB Board (DT)
    [ 208.527990] Call trace:
    [ 208.530432] dump_backtrace+0x0/0x140
    [ 208.534087] show_stack+0x14/0x20
    [ 208.537395] dump_stack+0xb4/0xf8
    [ 208.540703] panic+0x158/0x324
    [ 208.543750] mount_block_root+0x1d0/0x284
    [ 208.547752] mount_root+0x124/0x158
    [ 208.551232] prepare_namespace+0x15c/0x1c0
    [ 208.555321] kernel_init_freeable+0x210/0x22c
    [ 208.559671] kernel_init+0x10/0x100
    [ 208.563152] ret_from_fork+0x10/0x18
    [ 208.566721] SMP: stopping secondary CPUs
    [ 208.570643] Kernel Offset: 0x2b9897c00000 from 0xffff800010000000
    [ 208.576728] PHYS_OFFSET: 0xffffbf0c80000000
    [ 208.580904] CPU features: 0x0002,20806000
    [ 208.584904] Memory Limit: none
    [ 208.587953] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0) ]---
  • Tested with static IP as well, no difference.
  • Tried using the old NFSwatch tool on the Ubuntu NFS server, it shows no attempts of connection. It does show manual test connections.

As a side note, there are some worrying issues in the kernel log before the DHCP process:

[ 4.007485] ------------[ cut here ]------------
[ 4.012107] Your devicetree is out of date, please update it. The AQR107 family doesn't support XGMII, maybe you mean USXGMII.
[ 4.023535] WARNING: CPU: 2 PID: 1 at drivers/net/phy/aquantia_main.c:595 aqr107_config_init+0x94/0xa8
[ 4.032836] Modules linked in:
[ 4.035885] CPU: 2 PID: 1 Comm: swapper/0 Not tainted 5.4.3+gf811858 #1
[ 4.042492] Hardware name: LS1046A RDB Board (DT)
[ 4.047190] pstate: 60000005 (nZCv daif -PAN -UAO)
[ 4.051974] pc : aqr107_config_init+0x94/0xa8
[ 4.056324] lr : aqr107_config_init+0x94/0xa8
[ 4.060672] sp : ffff80001003ba10
[ 4.063978] x29: ffff80001003ba10 x28: ffff0009710b6000
[ 4.069284] x27: ffffab98a95c4000 x26: 0000000000001002
[ 4.074589] x25: ffff000971608800 x24: 0000000000000000
[ 4.079894] x23: 0000000000000000 x22: 000000000000000e
[ 4.085198] x21: ffff0009710b6000 x20: ffff0009710b64c0
[ 4.090503] x19: ffff000971608000 x18: 0000000000000010
[ 4.095808] x17: 0000000080cd1967 x16: 00000000b2afac86
[ 4.101113] x15: ffff000972475258 x14: 0720072007200720
[ 4.106418] x13: 0720072007200720 x12: 0000000000000001
[ 4.111723] x11: 0000000000000000 x10: 00000000000009a0
[ 4.117028] x9 : ffff80001003b750 x8 : ffff000972475800
[ 4.122333] x7 : ffff000972474f80 x6 : ffff0009739db900
[ 4.127638] x5 : 0000000000000000 x4 : 00000000000018b0
[ 4.132943] x3 : ffff5470ca174000 x2 : ffffab98a9cc3620
[ 4.138248] x1 : a7a7fcee37f9d100 x0 : 0000000000000000
[ 4.143552] Call trace:
[ 4.145991] aqr107_config_init+0x94/0xa8
[ 4.149993] phy_init_hw+0x54/0x70
[ 4.153387] phy_attach_direct+0xec/0x2a8
[ 4.157388] phy_connect_direct+0x24/0x78
[ 4.161391] of_phy_connect+0x4c/0x90
[ 4.165047] memac_init_phy+0x9c/0x138
[ 4.168789] dpa_start+0x2c/0x12c
[ 4.172096] dpa_eth_priv_start+0xb4/0xf4
[ 4.176099] __dev_open+0xc0/0x170
[ 4.179493] __dev_change_flags+0x160/0x1b8
[ 4.183669] dev_change_flags+0x20/0x60
[ 4.187498] ip_auto_config+0x264/0xe64
[ 4.191328] do_one_initcall+0x50/0x190
[ 4.195157] kernel_init_freeable+0x194/0x22c
[ 4.199508] kernel_init+0x10/0x100
[ 4.202988] ret_from_fork+0x10/0x18
[ 4.206555] ---[ end trace f7f7161a46513eb8 ]---

Can anyone help please?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,824 Views
Pavel
NXP Employee
NXP Employee

Perhaps CentOS and Ubuntu servers try to go to power save mode and it produces loosing of NFS connection.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply