Mini PCIe not detected on LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mini PCIe not detected on LS1043ARDB

1,810件の閲覧回数
mehdi-cubic
Contributor II

I have been unable to resolve the issue I posted here. Trying to use Sierra Modem EM9191 (also Telit FN990A) on LS1043ARDB.

Using M.2 to Mini PCIe adapter board (Techship MP301-ES) and u-boot does not detect the device on the PCI bus (see console output below).

I can successfully detect and run WiFi module 920NGW on this PCI bus (of course with different adapter board)

Please let me know if this is expected to work with the default configuration of nxp-qoriq build or if there are any changes that I can try on the configuration (e.g. RCW).

----------------

Using SERDES1 Protocol: 5205 (0x1455)
PCIe1: pcie@3400000 disabled
PCIe2: pcie@3500000 Root Complex: no link
PCIe3: pcie@3600000 Root Complex: no link

------------------

Thank you.

0 件の賞賛
返信
4 返答(返信)

1,725件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Can you check and tell us the PCIe LTSSM state[from PCI Express Link Control Register] at Uboot when you are connecting the Telit FN990A via M.2 to Mini PCIe adapter board ?

0 件の賞賛
返信

1,720件の閲覧回数
mehdi-cubic
Contributor II

Hello,
Thanks for the update. 
Yes sure, I will extract the value in this register and post it ASAP.

0 件の賞賛
返信

1,777件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 件の賞賛
返信

1,738件の閲覧回数
mehdi-cubic
Contributor II

I assume there has been no progress on this topic?

0 件の賞賛
返信