MCK AND VTT TERMINATION OF DDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCK AND VTT TERMINATION OF DDR4

3,181件の閲覧回数
Ellu24
Contributor III

I am designing a  new hardware using LS1046a.Now I am interfacing ddr4 with processor. I have few doubts regarding the VTT terminations.:

1) Can I use the decoupling capacitors as in attachment (reference board)?

2) or I have to use as specified in micron design rules of decoupling capacitors as: Use at least one low ESL cap or two standard decoupling caps for each four pack resistor network, Use at least one 4.7 µF cap at each end of the VTT island , Ensure the VTT island is properly decoupled with bulk decoupling. At least one bulk cap (47–220 µF) capacitor should be at each end of the island.

3) If it is specified as question 3,the  ho the circuit looks like?

4) which resistor and capacitor to use for MCK termination?

 

0 件の賞賛
返信
1 返信

3,171件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You can use the RDB as a reference. you may also take Micron design rules in consideration. also there is an application note for DDR4 AN5097 that you can use to determine the VTT decoupling caps and more.

0 件の賞賛
返信