Losing USB3 port on LS1046ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Losing USB3 port on LS1046ARDB

1,545件の閲覧回数
marco3181
Contributor III

Hello,

When I put an USB3 key on the LS1046A RDB, I lose the port, meaning there are no lights from the LED indicators for the 5V (D1 or D2). Overcurrent? Power Management?

I don't know what to look. The USB is reactivated with a lsusb -v (not the busybox one).

Any hint?

Thank you

Marc

ラベル(1)
0 件の賞賛
返信
1 返信

1,427件の閲覧回数
Pavel
NXP Employee
NXP Employee

It looks like that there is overcurrent on your board if this USB key is connected.Test your board using different USB device (USB memory stick and so on).
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信