LX2160ARDB-REV2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160ARDB-REV2

1,177 Views
Subhani7
Contributor II

Hi Team,

I am using LLDPUG_RevL5.15.71-2.2.0.

Machine : Lx2160ardb-rev2

After generating the RFS , KERNEL , Firmware

I flashed the images and it is working fine.

But now the same kernel and same build environment, after i did clean and build,

when i am trying to flash
I am getting the error as 

crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.32.0, boot status: 0x1)
Hit any key to stop autoboot: 0
=>
=> ls mmc 1:1
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
15798670 Image.gz
40838 fsl-lx2160a-rdb.dtb
35639 fsl-lx2160a-qds.dtb
35639 fsl-lx2160a-qds-lx2160ardb-rev2.dtb
43031040 Image
1015 lx2160ardb_boot.scr
40838 fsl-lx2160a-rdb-lx2160ardb-rev2.dtb
54244752 firmware_lx2160ardb-rev2_xspiboot.img
=> load mmc 1:1 0x92000000 firmware_lx2160ardb-rev2_xspiboot.img
54244752 bytes read in 174 ms (297.3 MiB/s)
=> sf erase 0x0 +$filesize && sf write 0x92000000 0x0 $filesize && reset
SF: 54263808 bytes @ 0x0 Erased: OK
device 0 offset 0x0, size 0x33bb590
SF: 54244752 bytes @ 0x0 Written: OK
resetting ...
NOTICE: BL2: v2.6(release):lf-5.15.71-2.2.0-0-g3c1583ba0-dirty
NOTICE: BL2: Built : 11:00:38, Nov 21 2022
NOTICE: Fixed DDR on board
NOTICE: DDR4 UDIMM with 1-rank 64-bit bus (x16)

NOTICE: 16 GB DDR4, 64-bit, CL=21, ECC on, 256B
NOTICE: BL2: Booting BL31
NOTICE: BL31: v2.6(release):lf-5.15.71-2.2.0-0-g3c1583ba0-dirty
NOTICE: BL31: Built : 11:00:38, Nov 21 2022
NOTICE: Welcome to lx2160ardb BL31 Phase


U-Boot 2022.04+fsl+g181859317bf (Nov 15 2022 - 06:28:05 +0000)

SoC: LX2160AE Rev2.0 (0x87361020)
Clock Configuration:
CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz
CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz
CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz
CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz
CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz
CPU15(A72):2000 MHz
Bus: 750 MHz DDR: 2900 MT/s
Reset Configuration Word (RCW):
00000000: 5077773c 24500050 00000000 00000000
00000010: 00000000 0c010000 00000000 00000000
00000020: 380001a0 00002580 00000000 1a009640
00000030: 08008000 00000001 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 000270b9 00000000
00000070: 0002003c 00010023
Model: NXP Layerscape LX2160ARDB Board
Board: LX2160AE Rev2.0-RDB, Board version: O, boot from invalid setting, xmap: 7
FPGA: v255.255
SERDES1 Reference: Clock1 = 100MHz Clock2 = 125MHz
SERDES2 Reference: Clock1 = 0MHz Clock2 = 0MHz
SERDES3 Reference: Clock1 = 0MHz Clock2 = 0MHz
I2C: Bus 0 has no device with address 0x77
PCA: No PCA9547 device found
I2C: Bus 0 has no device with address 0x77
PCA: No PCA9547 device found
core voltage not adjusted
DRAM: 15.9 GiB
DDR 15.9 GiB (DDR4, 64-bit, CL=21, ECC on)
DDR Controller Interleaving Mode: 256B
I2C: Bus 0 has no device with address 0x77
PCA: No PCA9547 device found
I2C: Bus 0 has no device with address 0x77
PCA: No PCA9547 device found
I2C: Bus 0 has no device with address 0x75
PCA: No PCA9547 device found
I2C: Bus 0 has no device with address 0x77
PCA: No PCA9547 device found
Using SERDES1 Protocol: 2 (0x2)
Using SERDES2 Protocol: 0 (0x0)
SERDES2[PRTCL] = 0x0 is not valid
Using SERDES3 Protocol: 0 (0x0)
SERDES3[PRTCL] = 0x0 is not valid
PCIe1: pcie@3400000 disabled
PCIe2: pcie@3500000 Root Complex: no link
PCIe3: pcie@3600000 disabled
PCIe4: pcie@3700000 disabled
PCIe5: pcie@3800000 disabled
PCIe6: pcie@3900000 disabled
Core: 43 devices, 19 uclasses, devicetree: separate
WDT: Started watchdog@23a0000 with servicing (30s timeout)
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from SPIFlash... SF: Detected gd55lb01ge with page size 256 Bytes, erase size 64 KiB, total 128 MiB
*** Warning - bad CRC, using default environment

EEPROM: Invalid ID (ff ff ff ff)
In: serial_pl01x
Out: serial_pl01x
Err: serial_pl01x
SEC0: RNG instantiated
Setting bus to 2
Valid chip addresses: 4F
VID: Core voltage after adjustment is at 3484 / 4096 mV
core voltage is adjusted.
Net:
Warning: DPMAC3@sgmii (eth0) using random MAC address - 42:87:e5:58:6c:56

Warning: DPMAC4@sgmii (eth1) using random MAC address - f6:ad:2b:be:bf:f9
eth0: DPMAC3@sgmii, eth1: DPMAC4@sgmii
SF: Detected gd55lb01ge with page size 256 Bytes, erase size 64 KiB, total 128 MiB
device 0 offset 0x640000, size 0x80000
SF: 524288 bytes @ 0x640000 Read: OK
device 0 offset 0xf00000, size 0x100000
SF: 1048576 bytes @ 0xf00000 Read: OK
device 0 offset 0xa00000, size 0x300000
SF: 3145728 bytes @ 0xa00000 Read: OK
device 0 offset 0xe00000, size 0x100000
SF: 1048576 bytes @ 0xe00000 Read: OK
crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.32.0, boot status: 0x1)
Hit any key to stop autoboot: 0
SF: Detected gd55lb01ge with page size 256 Bytes, erase size 64 KiB, total 128 MiB
device 0 offset 0x6c0000, size 0x40000
SF: 262144 bytes @ 0x6c0000 Read: OK
device 0 offset 0xd00000, size 0x100000
SF: 1048576 bytes @ 0xd00000 Read: OK
starting USB...
Bus usb3@3100000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
Bus usb3@3110000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb3@3100000 for devices... 1 USB Device(s) found
scanning bus usb3@3110000 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
MMC: no card present
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
Found U-Boot script /lx2160ardb_boot.scr
1015 bytes read in 1 ms (991.2 KiB/s)
## Executing script at 80000000
43031040 bytes read in 139 ms (295.2 MiB/s)
40838 bytes read in 0 ms
## Flattened Device Tree blob at 90000000
Booting using the fdt blob at 0x90000000
Loading Device Tree to 000000009fff3000, end 000000009fffff85 ... OK
"Synchronous Abort" handler, esr 0x96000006
elr: 0000000082004e00 lr : 0000000082004dc0 (reloc)
elr: 00000000fbd12e00 lr : 00000000fbd12dc0
x0 : 000000009fff55d0 x1 : 0000000016f82a8c
x2 : efbeaddeefbeadde x3 : 00000000efbeadde
x4 : 00000000fffffffc x5 : 000000009fffc8a2
x6 : 0000000000002590 x7 : 0000000000000003
x8 : 000000009fff3000 x9 : 0000000000000008
x10: 000000000000257c x11: 00000000fbb04cec
x12: 0000000000002534 x13: 0000000000000000
x14: 000000009fff3000 x15: 000000009fff3000
x16: 00000000fbd61e68 x17: 0000000000000000
x18: 00000000fbb09d90 x19: 0000000000002534
x20: 000000009fff3000 x21: 00000000fbdb093c
x22: 00000000fbdb1fe8 x23: 0000000000000000
x24: 00000000fbb365a8 x25: 00000000fbdd0f48
x26: 0000000000000000 x27: 00000000fbd13d1c
x28: 00000000fbb365d0 x29: 00000000fbb04db0

Code: a9425bf5 a8c47bfd d50323bf d65f03c0 (b8617803)
Resetting CPU ...

### ERROR ### Please RESET the board ###

Please help me to resolve the issue 

Tags (1)
0 Kudos
Reply
1 Reply

1,140 Views
yipingwang
NXP TechSupport
NXP TechSupport

=> pri xspi_bootcmd
xspi_bootcmd=echo Trying load from flexspi..;sf probe 0:0 && sf read $load_addr $kernel_start $kernel_size ; env exists secureboot &&sf read $kernelheader_addr_r $kernelheader_start $kernelheader_size && esbc_validate ${kernelheader_addr_r}; bootm $load_addr#$BOARD


=> run xspi_bootcmd

0 Kudos
Reply