[LX2160A] DDR4 not working normally

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LX2160A] DDR4 not working normally

1,489 Views
shinhakang
Contributor I

we successfully performed validation and confirmed that there was no fail. However, I created an expert code and applied it to the source, but ddr does not work normally.

When performing clock validation, we saw that appropriate clock delay values were selected in write leveling and read gate training. What register is this value stored in? We can't see the relevant value in the generated ddr_init.c. For ls1046, wrlvl control register exists - (DDR1_DDR_WRLVL_CNTL/2/3) . However, it does not exist on the lx2160a. If the lx2160a doesn't support it, this test seems meaningless. What should we do? Looking forward to your reply.

 

 

shinhakang_1-1677140758493.png

 

Attach log file as below :

log.zip

Thanks

0 Kudos
Reply
2 Replies

1,473 Views
shinhakang
Contributor I

Mrudang,

Then,, how about the attached log. We had passed QVSC validation, but not working normally.

Is there any checking point or idea to resolve.

Thanks,

Shinha.

0 Kudos
Reply

1,475 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @shinhakang,

LX2160A doesn't require WRLVL_START values. It is done automatically by LX2160A itself. That's the reason the reference manual doesn't have the details.

Regards,
Mrudang

0 Kudos
Reply