LSDK2108 SPI NOR FLASH JFFS2 initialize rootfs kernel panic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK2108 SPI NOR FLASH JFFS2 initialize rootfs kernel panic

1,620 Views
Hugh512
Contributor III

rootfs is flashed into SPI NOR flash

1. bootargs

set bootargs console=ttyS0,115200 noinitrd root=/dev/mtdblock4 rootfstype=jffs2 rootwait rw earlycon=uart8250,mmio,0x21c0500 quiet lpj=250000

2. rootfs is generated by

flex-builder -i mkrfs -r yocto:tiny
3. mkfs.jffs2 command
flexbuild_lsdk2108/build/rfs/rootfs_lsdk2108_yocto_tiny_arm64/target
 
sudo mkfs.jffs2 -o test.jffs2 -r target/ -e 0x10000 -s 0x1000 -n -l --pad=0x1000000
 
After booting into kernel, kernel crash:

INIT: version 2.99 booting
hwclock: can't open '/dev/misc/rtc': No such file or directory
Fri Mar 9 12:34:56 UTC 2018
hwclock: can't open '/dev/misc/rtc': No such file or directory
Configuring packages on first boot....
(This may take several minutes. Please do not power off the machine.)
Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...
update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)
Removing any system startup links for run-postinsts ...
INIT: Entering runlevel: 5
Starting random number generator daemon.
[ 4.840188] Unable to handle kernel paging request at virtual address ffffe36c00001590
[ 4.856120] Mem abort info:
[ 4.858916] ESR = 0x96000004
[ 4.866158] EC = 0x25: DABT (current EL), IL = 32 bits
[ 4.880121] SET = 0, FnV = 0
[ 4.883179] EA = 0, S1PTW = 0
[ 4.892139] Data abort info:
[ 4.895029] ISV = 0, ISS = 0x00000004
[ 4.904157] CM = 0, WnR = 0
[ 4.912141] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000085e11000
[ 4.924138] [ffffe36c00001590] pgd=0000000000000000, p4d=0000000000000000
[ 4.940141] Internal error: Oops: 96000004 [#1] PREEMPT SMP
[ 4.945724] Modules linked in:
[ 4.948789] CPU: 0 PID: 5 Comm: kworker/0:0 Not tainted 5.10.35-00002-gd06856fba47f-dirty #1
[ 4.957241] Hardware name: LS1012A RDB Board (DT)
[ 4.961964] Workqueue: events cache_reap
[ 4.965894] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--)
[ 4.971911] pc : cache_reap+0xcc/0x290
[ 4.975665] lr : cache_reap+0xfc/0x290
[ 4.979418] sp : ffff800010033ce0
[ 4.982735] x29: ffff800010033ce0 x28: ffff800010033d78
[ 4.988059] x27: ffff000000c27a00 x26: ffff80001252b550
[ 4.993383] x25: ffff00000004e140 x24: ffff800011f9f758
[ 4.998708] x23: ffff80001252b570 x22: ffff000001175500
[ 5.004032] x21: 0000000000000080 x20: 0000000000000000
[ 5.009356] x19: ffff800012496980 x18: fffffdffffe47708
[ 5.014680] x17: ffff0000011a1c88 x16: ffff0000011a1ca8
[ 5.020005] x15: 0001000000000000 x14: fffffdffffe00000
[ 5.025329] x13: dead000000000100 x12: dead000000000122
[ 5.030652] x11: ffff0000011dc040 x10: 0000000000000001
[ 5.035976] x9 : ffff0000011dc040 x8 : ffff0000011a1c80
[ 5.041300] x7 : 0000000000000006 x6 : ffff800027c53000
[ 5.046624] x5 : 0000000000000000 x4 : ffff000000c27a60
[ 5.051948] x3 : ffff800010033ce0 x2 : 0000000000000000
[ 5.057272] x1 : ffff800027c53000 x0 : ffffe36c00001590
[ 5.062595] Call trace:
[ 5.065046] cache_reap+0xcc/0x290
[ 5.068452] process_one_work+0x1bc/0x338
[ 5.072467] worker_thread+0x50/0x420
[ 5.076135] kthread+0x154/0x158
[ 5.079367] ret_from_fork+0x10/0x34
[ 5.082950] Code: f9400416 f94032c0 b40000e0 f8616b02 (f862d806)
[ 5.089055] ---[ end trace 4188919bba8dcb43 ]---
[ 5.844155] random: crng init done
Starting OpenBSD Secure Shell server: sshd
generating ssh RSA host key...
generating ssh ECDSA host key...
generating ssh ED25519 host key...
[ 13.214387] ------------[ cut here ]------------
[ 13.219030] kernel BUG at net/netlink/af_netlink.c:1354!
[ 13.224352] Internal error: Oops - BUG: 0 [#2] PREEMPT SMP
[ 13.229847] Modules linked in:
[ 13.232913] CPU: 0 PID: 322 Comm: sshd Tainted: G D 5.10.35-00002-gd06856fba47f-dirty #1
[ 13.242324] Hardware name: LS1012A RDB Board (DT)
[ 13.247037] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)
[ 13.253061] pc : netlink_has_listeners+0x9c/0xa0
[ 13.257689] lr : __sk_free+0x94/0xd8
[ 13.261266] sp : ffff800010033c60
[ 13.264583] x29: ffff800010033c60 x28: ffff000000b0c1c0
[ 13.269908] x27: 0000000000000000 x26: 0000000000000000
[ 13.275232] x25: 0000000000000000 x24: 0000000000000000
[ 13.280556] x23: ffff0000000272e0 x22: ffff0000005d5cc0
[ 13.285880] x21: 0000000000000000 x20: ffff000000b4fc68
[ 13.291204] x19: 0000000000000004 x18: 0000000000000000
[ 13.296528] x17: 0000000000000000 x16: 0000000000000000
[ 13.301852] x15: 0000000000000000 x14: 0000000000000000
[ 13.307176] x13: 0000000000000000 x12: 0000000000000000
[ 13.312500] x11: 0000000000000000 x10: 0000000000000000
[ 13.317823] x9 : 0000000000000000 x8 : 0000000000000000
[ 13.323147] x7 : ffff000000b0c1c0 x6 : ffff000000b4fb8c
[ 13.328470] x5 : 0000000000000001 x4 : 0000000000000000
[ 13.333794] x3 : ffff800027c53000 x2 : ffff000000b0c1c0
[ 13.339117] x1 : 0000000091908f87 x0 : ffff000001167800
[ 13.344442] Call trace:
[ 13.346892] netlink_has_listeners+0x9c/0xa0
[ 13.351168] __sk_free+0x94/0xd8
[ 13.354399] sk_free+0x34/0x80
[ 13.357458] sk_common_release+0x98/0x110
[ 13.361476] udp_lib_close+0x10/0x20
[ 13.365058] inet_release+0x44/0x70
[ 13.368552] inet6_release+0x34/0x50
[ 13.372131] __sock_release+0x44/0xc0
[ 13.375796] sock_close+0x18/0x28
[ 13.379118] __fput+0x78/0x230
[ 13.382174] ____fput+0x10/0x20
[ 13.385321] task_work_run+0x80/0x140
[ 13.388989] do_notify_resume+0x23c/0x6e8
[ 13.393004] work_pending+0xc/0x3a8
[ 13.396500] Code: f94013f5 a8c37bfd d50323bf d65f03c0 (d4210000)
[ 13.402604] ---[ end trace 4188919bba8dcb44 ]---
[ 13.407229] note: sshd[322] exited with preempt_count 1
Segmentation fault
hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting syslogd/klogd: done

NXP LSDK tiny 2108 (based on Yocto)
TinyLinux login: [ 14.326450] ------------[ cut here ]------------
[ 14.331108] WARNING: CPU: 0 PID: 0 at kernel/rcu/tree.c:624 rcu_eqs_enter.isra.0+0x84/0x90
[ 14.339386] Modules linked in:
[ 14.342452] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G D 5.10.35-00002-gd06856fba47f-dirty #1
[ 14.352124] Hardware name: LS1012A RDB Board (DT)
[ 14.356837] pstate: 20000085 (nzCv daIf -PAN -UAO -TCO BTYPE=--)
[ 14.362855] pc : rcu_eqs_enter.isra.0+0x84/0x90
[ 14.367394] lr : rcu_idle_enter+0x10/0x20
[ 14.371407] sp : ffff800012493e10
[ 14.374724] x29: ffff800012493e10 x28: 0000000085e20018
[ 14.380050] x27: 0000000000000000 x26: ffff000001067880
[ 14.385374] x25: 0000000000000018 x24: 0000000355ebe350
[ 14.390699] x23: 0000000000000000 x22: ffff000001067880
[ 14.396023] x21: ffff000039bf3640 x20: ffff000001067898
[ 14.401348] x19: 0000000000000000 x18: 0000000000000002
[ 14.406673] x17: 0000000000000000 x16: 0000000000000000
[ 14.411997] x15: 0000b10a67d94e94 x14: 0000000000000322
[ 14.417321] x13: 0000000000000001 x12: 0000000000000019
[ 14.422645] x11: 071c71c71c71c71c x10: 0000000000000001
[ 14.427970] x9 : ffff000039bf39cc x8 : 0000000000000007
[ 14.433294] x7 : 000000007fffffff x6 : 0000000147bc849d
[ 14.438618] x5 : 00ffffffffffffff x4 : 0000000000000015
[ 14.443942] x3 : 4000000000000002 x2 : 4000000000000000
[ 14.449267] x1 : ffff800011fa3540 x0 : ffff000039bf6540
[ 14.454591] Call trace:
[ 14.457042] rcu_eqs_enter.isra.0+0x84/0x90
[ 14.461231] rcu_idle_enter+0x10/0x20
[ 14.464900] cpuidle_enter_state+0x24c/0x2f0
[ 14.469175] cpuidle_enter+0x38/0x50
[ 14.472756] call_cpuidle+0x1c/0x40
[ 14.476249] do_idle+0x204/0x268
[ 14.479479] cpu_startup_entry+0x24/0x68
[ 14.483409] rest_init+0xd8/0xe8
[ 14.486643] arch_call_rest_init+0x10/0x1c
[ 14.490745] start_kernel+0x4b4/0x4f0
[ 14.494410] ---[ end trace 4188919bba8dcb45 ]---

 

 

0 Kudos
Reply
1 Reply

1,590 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

What board are you using?

We have precompiled images ready to be installed on your board, please try that images.

We have instructions on how to deploy images on your board, please follow those instructions for your board.

 

Supported Boards | QorIQ SDK v2.0-1703 Documentation | NXP Semiconductors

0 Kudos
Reply