LSDK1906 build error---gzip: ramdisk_rootfs_arm64.ext4.gz: unexpected end of file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK1906 build error---gzip: ramdisk_rootfs_arm64.ext4.gz: unexpected end of file

2,358 Views
lixiaofan
Contributor II

I use flexbuild_lsdk1906_update_290719.tgz , my host machine is CentOS7, so I unpack this pkgs, and then use

flex-builder docker 

this create a docker image for fbubuntu18.04, and then enter it, then I 

source setup.env

flex-builder -m ls1043ardb -a arm64

evetythins is ok, but at the last occur errors , please help me!!

... 

cd plat/nxp/tools; make clean ; cd -;
make[3]: Entering directory '/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/packages/firmware/atf/plat/nxp/tools'
make[3]: Leaving directory '/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/packages/firmware/atf/plat/nxp/tools'
/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/packages/firmware/atf
make[2]: Leaving directory '/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/packages/firmware/atf'
-rw-r--r--. 1 root root 44756 Oct 18 08:05 /home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/build/firmware/atf/ls1043ardb/bl2_nor.pbl
-rw-r--r--. 1 root root 1095353 Oct 18 08:05 /home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/build/firmware/atf/ls1043ardb/fip_uefi.bin
Build ATF for ls1043ardb norboot in /home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/build/firmware/atf/ls1043ardb [Done]
make[1]: Leaving directory '/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/packages/firmware'
make: Leaving directory '/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906'
Generating norboot composite firmware image for ls1043ardb ...
/home/lee/zData/Projects/lsdk-1906/flexbuild_lsdk1906/build/images/lsdk_linux_arm64_LS_tiny.itb not exist, generating it ...
INSTRUCTION: mklinux
DESTARCH: arm64
PORTFOLIO: LS
CONFIGLIST: build_lsdk.cfg

gzip: ramdisk_rootfs_arm64.ext4.gz: unexpected end of file

Labels (2)
2 Replies

2,137 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Xiaofan Lee,

Probably there is networking problem to download file ramdisk_rootfs_arm64.ext4.gz completely.

Please check whether packages/rfs/ramdiskrfs/ramdisk_rootfs_arm64.ext4.gz is about 17M. If no, please remove it and  run flex-builder command to download it again.

Thanks,

Yiping

0 Kudos
Reply

2,137 Views
johannes_renkl
Contributor I

Oh I think, I just asked the same question here: ramdisk rootfs arm64 missing - now I guess its a duplicate...

The file in question vanished from your server...

0 Kudos
Reply