LS2088A PCIe and NFA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2088A PCIe and NFA

1,435 Views
mmcminn
Contributor I

Is there a high speed data path between the PCIe bus and the NFA engine in the LS2088A and is it able to run at the rated 10Gb/s speed.

Labels (1)
0 Kudos
Reply
1 Reply

1,258 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Michael McMinn,

QDMA can go across PCIe to access data, the PCIe EP can use QDMA to access data/buffers across PCIe to RC.

NFA engine(PME) belongs to DPAA, which is primarily for Ethernet because it has portal interface to QBMAN. The PME de-queues data from its QMAN hardware portal based on FQ configuration. QBMAN can be used to improve performance for data that are come in through the PCI bus.

PME supports ~10 Gbps data scanning.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply