LS1046ARDB pinmux RCW setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ARDB pinmux RCW setting

ソリューションへジャンプ
3,396件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team.

We have an External WDT device and the Enable/Trigger line connect to GPIO2_2/GPIO2_03 respectively.

Can we set pinmux in RCW file ? How to do it ?

ラベル(2)
0 件の賞賛
返信
1 解決策
3,390件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is needed to add into the ".rcw" file the following line:

SPI_BASE=2

Please note that SPI cannot be used in this case because SPI_SCK is available only when RCW[SPI_EXT]=0 and RCW[SPI_BASE]=0.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,379件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team.

Theree are another question.

We want to force pull-high or pull-low the Enable/Trigger pins in U-Boot.

Do you have any suggestion for us ?

0 件の賞賛
返信
3,376件の閲覧回数
ufedor
NXP Employee
NXP Employee

>Theree are another question.

Please create new Community question.

0 件の賞賛
返信
3,391件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is needed to add into the ".rcw" file the following line:

SPI_BASE=2

Please note that SPI cannot be used in this case because SPI_SCK is available only when RCW[SPI_EXT]=0 and RCW[SPI_BASE]=0.

0 件の賞賛
返信
3,384件の閲覧回数
charleshuang
Senior Contributor II

OK, thank you, I try it first .

0 件の賞賛
返信