LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse

1,442件の閲覧回数
Em31
Contributor II

Hi all,

I am trying to access theLS1046ARDB console connection from the UART to the COM by using the RJ45-to-DB9F cable.

I have changed the SW4[4] on my LS1046ARDB board to 0 and configured the teraterm configure serial speed at 115200, but there is no connection that can be established.

Could you please tell me:

1. Is there any other setup I need to configure to make it work, etc., driver?

If not, can you suggest another method to make the connection work besides connecting to the front port?

Thanks in advance.

 

0 件の賞賛
返信
1 返信

1,412件の閲覧回数
Chanh
Contributor III

Hi,

For the Teraterm, did you configure all the parameters as mentioned in the Getting Start Guide?

I use an RJ45-to-USB cable instead, and it works for me. I only need to install the USB driver on my Win10 pc.

タグ(1)
0 件の賞賛
返信