[LS1046A]kernal panic issue when run iperf3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1046A]kernal panic issue when run iperf3

2,527件の閲覧回数
richard_guo
Contributor I

Hi NXP,

I have some questions about kernal panic.  I use LS1046A as the server side, and my PC as the client side.

PC through telnet and input commands: iperf3 -c 192.168.1.254 -t 600 -R

After about 10 seconds of testing, iperf is stopped, and an error log was seen. Also I have the same problem using both WAN and LAN ports, please refer to the attached file for detailed logs.

 

Thanks,

Richard Guo

ラベル(1)
0 件の賞賛
返信
1 返信

2,480件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Which version NXP LSDK are you using? Or where did you get Linux Kernel source code?

Would you please send your Linux Kernel configuration file to me to do more investigation?

0 件の賞賛
返信