LS1046A QSPI signal state when PORESET_B asserted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A QSPI signal state when PORESET_B asserted

1,822件の閲覧回数
sabine_s
Contributor III

For the LS1046A, when PORESET_B is asserted, are all QSPI signals in high impedance state?

I am wondering if I can program QSPI RCW/PBI/boot flash using an external master if I apply power and keep PORESET_B asserted. Any problems doing it this way?

ラベル(1)
1 返信

1,667件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes, external master can program SPI Flash connected to QSPI when PORESET_B is asserted.