LS1046 does not boot from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 does not boot from SD card

1,639 Views
douglassilva
Contributor II

I am trying to boot from SD card, LS1046 using OK1046A-C2 Single Board Computer from forlinx.

I am flashing the SD card using the following command

flex-installer -i auto -m ls1046ardb -d /dev/sdq -p 4P=128M:2G:8G:-1

And it installs all partitions into SD card successfully(attached file showing instalation finishing successfully)

But then when I connect it to OK1046-C2 board and try to boot these are the kernel messages I get(full boot log attached)

[ 3.108076] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 3.108968] Freescale USDPAA process IRQ driver
[ 3.112360] optee: probing for conduit method.
[ 3.125802] optee: revision 2.6
[ 3.126122] optee: initialized driver
[ 3.138321] NET: Registered protocol family 26
[ 3.142792] u32 classifier
[ 3.145510] input device check on
[ 3.149185] Actions configured
[ 3.152903] Initializing XFRM netlink socket
[ 3.157214] NET: Registered protocol family 10
[ 3.162081] Segment Routing with IPv6
[ 3.165785] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.171894] NET: Registered protocol family 17
[ 3.176352] NET: Registered protocol family 15
[ 3.180809] Bridge firewalling registered
[ 3.184924] 8021q: 802.1Q VLAN Support v1.8
[ 3.189111] lib80211: common routines for IEEE802.11 drivers
[ 3.193552] mmc0: error -110 whilst initialising SD card
[ 3.200103] 9pnet: Installing 9P2000 support
[ 3.204387] tsn generic netlink module v1 init...
[ 3.209119] Key type dns_resolver registered
[ 3.213550] registered taskstats version 1
[ 3.217654] Loading compiled-in X.509 certificates
[ 3.223313] Btrfs loaded, crc32c=crc32c-generic
[ 3.229821] ALSA device list:
[ 3.232784] No soundcards found.
[ 3.236370] Waiting for root device PARTUUID=c52a6a85-04...
[ 3.339452] random: crng init done

Tags (1)
0 Kudos
Reply
2 Replies

1,617 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Which version of LSDK are you testing?

0 Kudos
Reply

1,611 Views
douglassilva
Contributor II
I am testing with LSDK 2108, but I did not had successfull results with 2012 either.
0 Kudos
Reply