LS1043a Interrupt Priority

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043a Interrupt Priority

2,032件の閲覧回数
notshure
Contributor IV

Hello everyone,
I found out thanks to the document QorIQ LS1043A Reference Manual, Rev. 6, 07/2020, that the ls1043a processor has the following list of external interrupt input signals:

Capture.PNG

These interrupt input signals are connected to the Arm generic interrupt controller (GIC-400).

I wanted to know if there was a concept of priority over interrupts among these interrupt input signals.
If priority is present, is the priority of these interrupts programmable?

0 件の賞賛
返信
1 返信

2,001件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

The priority of these interrupts can be set using Interrupt Priority Registers. Refer Table 3-2 Distributor register summary  in GIC-400 Technical Reference Manual ( https://developer.arm.com/documentation/ddi0471/b). Also refer ARM Generic Interrupt Controller Architecture Specification for Priority registers.

0 件の賞賛
返信