LS1043ARDB 10min reboot loop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB 10min reboot loop

1,698件の閲覧回数
xarowubas
Contributor III

I have an ls1043ARDB and am just getting started to get some Linux with a recent kernel (4.14+) running on it. I started off with LSDK1809 and the Ubuntu rfs + 4.14.47 kernel keeps rebooting every 10min. I have tried several other modern kernels in the same rfs, a few different 4.14 and a 4.19. In all of them the system reboots after pretty much exactly 10min, if not interacted with. With an open ssh i sometimes see more.

4.1 ran for several days on that rfs, and also in an rfs from an older SDK (yocto morty based)

0 件の賞賛
返信
3 返答(返信)

1,546件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following pages about Linux rebooting every a few time:

https://www.agix.com.au/shutdown-or-reboot-a-linux-server-10-minutes-from-now/

 

https://www.cyberciti.biz/faq/crontab-every-10-min/


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,546件の閲覧回数
xarowubas
Contributor III

I do not want the machine to reboot. The constant rebooting is the issue i am trying to report. And it is not reboot but rather "reset", i just get back into the boot-loader without any message.

0 件の賞賛
返信

1,546件の閲覧回数
xarowubas
Contributor III

4.9 kernels have the same issue, i now also tried the latest OpenWRT for it. So another rfs and yet another 4.9 kernel ... same thing

0 件の賞賛
返信