LS1043A interface with DDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A interface with DDR4

2,181 Views
Pamid
Contributor II

We would like to use   LS1043A custom board with  DDR4 in 16bit mode. Regarding this  Please confirm the interface connections between LS1043A and  DDR4 as per attached doc.

What is the use of  MA14\MBG1 in 16 bit mode.

0 Kudos
Reply
1 Reply

2,140 Views
yipingwang
NXP TechSupport
NXP TechSupport

the diagram looks correct. MA14/MBG1 is used when x8 DDR4 DRAM chips are used (x8 has 4 bank groups). x16 DDR4 does not use the BG1 (it has two bank groups)

0 Kudos
Reply