LS1043A and family transient response

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A and family transient response

576 Views
abhinav
Contributor I

Hi,

I have a question pertaining more specifically to the 1043A as well as the other LS10XXA devices. The datasheet describes either +50mV/-30mV or +/-30mV on most 1.0V rails for the recommended values. My question specifically is: is this the total range or just the DC variation range. Is there another 30mV for transient variation effectively making this +80mV/-60mV and +/-60mV or is it strictly as described.

Thanks,

Abhinav.

Tags (2)
0 Kudos
Reply
1 Reply

494 Views
andrei_skok
NXP Employee
NXP Employee

It is the total range, transient variation is included.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply