IBIS Simulation Model QSPI-IF of LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IBIS Simulation Model QSPI-IF of LS1046A

1,358件の閲覧回数
michaelfrings-b
NXP Employee
NXP Employee

Ctm is doing signal Integrity simulations on the QSPI-If of our LS1046A design.

 They are using the IBIS model ‘ls1046_vop3_9april2016.ibs’

 For the QSPI-IF I found the models ‘lvcmos18_ssr_fc_out’ or ‘lvcmos18_fsr_fc_out’ for output pins and ‘lvcmos18_fsr_fc_io’ or ‘lvcmos18_ssr_fc_io’ for I/O-pins.

 They haven’t found a possibility to select between one of the two I/O characteristics in the Reference Manual nor in the Datasheet.

 Question:

Is there a possibility to select between the different driving strengths or it is fixed?

If fixed, which one is used?

0 件の賞賛
返信
1 返信

1,195件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The IBIS model you are using is not most recent and indeed contains model selector "lvcmos" for these pins.Your understanding is correct, impedance is fixed and, therefore, this model selector is not necessary. For QSPI pins actual model will be model with *fsr* suffix. 

Please submit a ticket to online technical support to get most recent IBIS model, which does not have this problem.

How to submit a new question for NXP Support 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信