LS1043A USB compliance test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A USB compliance test

2,023件の閲覧回数
CurtisChen
Contributor I

Hello,

      Is there any LS1043A USB certification note for doing USB 2.0/3.0 compliance test?

      I am not sure is there any tool or method to do full USB compliance test? (eg. USB PHY register ...etc)

      Please share me the related document for my reference.

 

      Thanks.

      

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,623件の閲覧回数
micha
Contributor II

Hello 

DId you get an answer from NXP ?

I want to test a LS1046 USB interface,

it was easy with an T1046, just setting two register and we could measure eye diagram's

Regards,

Mike

0 件の賞賛
返信

1,819件の閲覧回数
Vivekn92
Contributor I

Hello,

I have the same question as above, are there any guidelines on setting LS1043 registers to force the USB into different states to perform compliance testing and check the eye diagram?

Regards
Vivek 

0 件の賞賛
返信