LS1043A - I2C module baremetal project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A - I2C module baremetal project

1,604件の閲覧回数
babatejbotcha
Contributor I

Need to enable the INA220 current sensor through I2C module of LS1043A RDB,
Could you please share me the code of I2C initilization, transfer, receive sequences inorder to access the INA220 digital current sense amplifier.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,473件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 8.3.4.3 od NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This Section contains description for using the INA220 Linux driver.

 

See also the Section 8.4.1.

 

See the Chapter 11.4 of NXP LSDK 18.03 documentation about using the INA220 Linux driver:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.03.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信