LS1043A GPCM Porgram 模式

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A GPCM Porgram 模式

ソリューションへジャンプ
2,487件の閲覧回数
shawn_tao
Contributor I

你好,LS1043A的GPCM模式下,non-burst的写时序,可否利用WE的下降沿作为采样数据的标准?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,407件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I use the WE falling edge to sample the programmed data?

Yes, you can.

Refer to the QorIQ LS1043A Reference Manual, Figure 25-43. Normal GPCM program operation - non-burst mode

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,407件の閲覧回数
ufedor
NXP Employee
NXP Employee

IFC_CSORn_GPCM[BURST_LEN]=000 Non-burst mode

Refer to the QorIQ LS1043A Reference Manual,25.3.7 Chip-Select Option register - GPCM (IFC_CSORn_GPCM)

0 件の賞賛
返信
2,407件の閲覧回数
shawn_tao
Contributor I

in non-burst mode, Can I use the WE falling edge to sample the programmed data? 

or must use a high speed clock to sample the WE falling edge as a start and then sample the data during the TWP cycle, any other method if I don't have such a high speed clock in my design?

0 件の賞賛
返信
2,408件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I use the WE falling edge to sample the programmed data?

Yes, you can.

Refer to the QorIQ LS1043A Reference Manual, Figure 25-43. Normal GPCM program operation - non-burst mode

0 件の賞賛
返信