LS1043A DDR3L data-bit swap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A DDR3L data-bit swap

1,232 Views
tom_derks
Contributor I

Hello,

I have a question regarding data-bit swap within byte-lan in combination with write levelling for the LS1043A

Does write level support mean the DQ0 pin cannot be swapped? Or is the functionality supported on all pins.

If memory device also matters, we plan to use: Micron MT41K512M16

best regards,

Tom

0 Kudos
Reply
1 Reply

1,185 Views
r8070z
NXP Employee
NXP Employee

It is possible to swap any bits within a byte lane. Please refer to the nxp appnote AN3940, Table 1. “DDR3 Designer Checklist”, No 45.

0 Kudos
Reply