LS1043 Hardware design requirements for Secure Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 Hardware design requirements for Secure Boot

2,429 Views
vinodstanly
Contributor I

What are the hardware design considerations required for Secure Boot in LS1043 Platform?

LS1043 Datasheet mentions the following 2 Items

Item-1

"TA_PROG_SFP must be supplied 1.8 V and the chip must operate in the specified fuse programming temperature range only during secure boot fuse programming. For all other operating conditions, TA_PROG_SFP must be tied to GND"

Item-2

For secure boot fuse programming, use the following steps:
1. After the negation of PORESET_B signal, drive TA_PROG_SFP = 1.8 V after a
required minimum delay as listed in
Table 7.
2. After the fuse programming is complete, it is required to return TA_PROG_SFP =
GND before the system is power cycled (PORESET_B assertion) or powered down.

-------------------------------------------------------------------------------------------------------------------

 LS1043ARDB (Reference board) has a J13 Jumper option connected to 1.8V.  Operated Manually.

Is this the only requirement in hardware for Secure boot implementation ? Any other requirements in Hardware design to implement Secure BOOT for LS1043?

 

 

Labels (1)
0 Kudos
Reply
3 Replies

2,415 Views
vinodstanly
Contributor I

Hi Bulat,

Thanks for your quick response.

  1. Switching of TA_PROG_SFP signal is now done Manually, Is there any reference that this feature is automated by a program or additional components.
  2. The above programming for Secure boot feature is limited to 6 times in the life time of a processor, right. What happens after that, will the device become read only?
  3. Apart from programming, for LS1043 to work with the Secure Boot feature; any other Hardware Connections, additional Components to be considered in the design.

 

0 Kudos
Reply

2,404 Views
Bulat
NXP Employee
NXP Employee

1. Yes, on our boards it is done in a manual way. You can design your own circuit which will switch the power on/off.
2. Limit of 6 times relates to fuse programming. After that you will not be able to change/re-program fuses.
3. No, besides mentioned in 1) above.

 

0 Kudos
Reply

2,424 Views
Bulat
NXP Employee
NXP Employee

Yes, switching of TA_PROG_SFP signal is the only hw design requirement for secure boot fuse programming.

Regards,

Bulat

 

0 Kudos
Reply