LS1043 DDR training error 0x3100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 DDR training error 0x3100

1,488 Views
zhy666
Contributor I

our boards are using the on-board DDR 1600MHz (micron)

the weird part is that when we only use single rank(2GB)the board could boot up and normally work ,but when we change to the two ranks (4GB)it print the error shows in the file down below 

i have already check the power ,initial timing and reset  but i cant find any clue could lead to this

any suggestion?

Tags (1)
0 Kudos
Reply
1 Reply

1,433 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please go to atf source code folder components/firmware/atf/, please modify plat/nxp/soc-ls1043a/ls1043ardb/ddr_init.c according to your custom board.

0 Kudos
Reply