LS1028ARDB Board GPIO Pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028ARDB Board GPIO Pins

1,141件の閲覧回数
SoccerMom
Contributor II

Hello,

I am using the LS1028ARDB board and have turned on the GPIOs with RCW[EC1_SAI4_5_PMUX] set to 1. I wanted to know if there is a document somewhere that shows me where the GPIO pins are. I want to use multiple GPIOs with that RCW change, but have no board document to show what pins it corresponds to on the board.

Thanks!

タグ(1)
0 件の賞賛
返信
1 返信

1,127件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

You can download the Schematic of the board by following the link:

Layerscape LS1028A Reference Design Board | NXP Semiconductors

Is the schematic of the entire board to see where are connected the pins in the processor.

0 件の賞賛
返信