LS1028A new design without CPLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A new design without CPLD

Jump to solution
2,010 Views
mkraj
Contributor III

Dear NXP expert

We are planning to go for a new LS1028A based board design without CPLD. We want to implement all reset and control outside CPLD.

Is there any dependency on firmware? Is it mandatory to use CPLD?

Thank you

With Regards

0 Kudos
Reply
1 Solution
1,977 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

View solution in original post

0 Kudos
Reply
2 Replies
1,978 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

0 Kudos
Reply
1,970 Views
mkraj
Contributor III
Dear Mrudang

Thank you verymuch for your valuable reply.

1. In LS1028A RDB , Few registers are implemented (board control and status register) in CPLD.

If we are removing CPLD, Any major software change is required?

2. Is it ok to go without these BCSR - Board Control / Status Registers in CPLD?

With Regards

Krishnam Raju M
0 Kudos
Reply