LS1028A RCW generation errors in Code Warrior tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A RCW generation errors in Code Warrior tool

2,477件の閲覧回数
kumar_086
Contributor IV

Dear Experts,

The compiled RCW from the flex build tool path rcw_1500_gpu600.bin  (<flexbuild_dir>/packages/firmware/rcw/ls1028ardb/R_SQPP_0x85bb) imported in Codewarrior v11.5.0 and observed some of the required fields having invalid or custom values and tool giving an error when compiling with this.

Error message: PBL image was not generated as it contains error. Fix the problems or check 'ignore constraints' button to generate the PBL image.

As attached an example of RCW error field CGA_PLL1_RAT [31-26] : selected value 0x1111 (a valid value as per processor manual).

Please help!

Thanks in advance.

0 件の賞賛
返信
1 返信

2,469件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I imported LSDK default RCW file rcw_1500_gpu600.bin in CW 11.5.5, also encountered similar problem as you. There is problem with the CW QCVS tool, please click "Enable/Disable error checking" button to select "Skip error checking". Please refer to the following screenshot.

yipingwang_0-1655196697468.png

 

0 件の賞賛
返信