LS1028A IEEE1588 support with Phy timestamping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A IEEE1588 support with Phy timestamping

548 Views
pb3
Contributor II

Hello, I have a question regarding IEEE1588 support on LS1028A, I browsed through the available materials but did not find the answer for my question, namely -does Felix switch driver or MAC driver (I'm not sure which one) support IEEE1588 with timetamping being preformed by Ethernet Phy instead of MAC layer? I'm wondering because in theory using Phy timestamping should allow to achieve better precision since it's closed to the line. At least in theory. How does it work on this SoC?

0 Kudos
Reply
1 Reply

498 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

No — on LS1028A, IEEE 1588/PTP timestamping is documented as being done by the SoC’s internal Ethernet hardware (ENETC MAC or Felix switch MAC/PTP block), not by the external Ethernet PHY.  IEEE 1588 timestamping is handled internally by the ENETC/Felix MAC-side PTP hardware and separate PHC blocks, not by external PHY-based packet timestamping.

 

Regards

0 Kudos
Reply