LS1028 Pinmux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028 Pinmux

9,490 Views
nybwc
Contributor II

Seems PinMux tool in Codewarrior 11.5.0 for LS1028a is not correct?  several pins are different from the datasheet.

 

5 Replies

9,452 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @nybwc 

Hope this post finds you well,

Could you please specify which pinouts are incorrect?

I have CodeWarrior version 11.5.0 and have verified several pins and they are correct.

I am using the QorIQ LS1028A/LS1018A, Rev. 0, 12/2019 datasheet.

Attached in the case there is an image in reference of one of the pins I have chosen.

Best Regards,

Hector Villarruel

0 Kudos
Reply

9,444 Views
nybwc
Contributor II

Here are a few conflict I saw.  Not sure if this is all.  Basically I saw differences and I could trust the pinmux.

 

 

9,313 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @nybwc 

Hope this post finds you well,

This post is to inform you that we keep working on this case.

Regarding the "Analog" image in reference attached by you, this signal does not appear since they are  for internal use as signal Description section of the datasheet indicates " Internal Use Only ". This signal is related to the analog part of the PLL and the internal regulator of the device, I highly recommend you to follow their respective note for the FA_ANALOG_PIN  signal." 15. These pins must be pulled to ground (GND)." 

I'll keep you informed.

Best Regards,

Hector Villarruel Silvadoray

0 Kudos
Reply

9,283 Views
nybwc
Contributor II

no problem we are not using this pin I was just pointing out differences between datasheet and pinmux

9,182 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @nybwc

Hope this post finds you well,

Apologies for delay.
SWITCH_S*_* signals are internal-only, not for showing in any customer documentation. Therefore, it is not present in data sheet and Reference manual.
The QCVS pin tool is not updated and shows these internal pins.
As per the tools team, it will not be updated.

Have a great day.

Best Regards,

Hector Villarruel

0 Kudos
Reply