LS1023A IFC Integrated Flash Controller can't find SRAM Base address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1023A IFC Integrated Flash Controller can't find SRAM Base address

跳至解决方案
858 次查看
Salman_tahir
Contributor I

Hi, I am working on LS1023A's peripheral  IFC (Integrated Flash Controller)

Question: How can be found the SRAM base address used by the IFC for the NAND Flash device?

                I am interfacing MT29F8G08ABBCAH4 with IFC.   

 

0 项奖励
回复
1 解答
807 次查看
yipingwang
NXP TechSupport
NXP TechSupport
4 回复数
824 次查看
Salman_tahir
Contributor I

Thanks @yipingwang 

0 项奖励
回复
822 次查看
Salman_tahir
Contributor I
Thanks @yipingwang

I have the following ifc node in the DTS file

&ifc {
status = "okay";
#address-cells = <2>;
#size-cells = <1>;
/* NAND Flashes, SRAM and FPGA on board */
//ranges = <0x0 0x0 0x00000006 0x20000000 0x40000000
// 0x1 0x0 0x0 0x60000000 0x00080000
// 0x2 0x0 0x0 0x70000000 0x00020000>;
ranges = <0x0 0x0 0x0 0x70000000 0x10000000
0x1 0x0 0x0 0x60000000 0x00080000
0x2 0x0 0x0 0x60100000 0x00020000>;

nand@0,0 {
compatible = "fsl,ifc-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x0 0x0 0x10000000>;
};

sram@1,0 {
compatible = "renesas,rmlv0416egsb";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x1 0x0 0x00080000>;
};

fpga: board-control@2,0 {
compatible = "nec,gcd-cp30-fpga";
reg = <0x2 0x0 0x0020000>;
};
};

Its mean NAND device is attached with CS0 and NAND_BASE base address is 0x70000000

is this understanding correct?
0 项奖励
回复
808 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

830 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The base address of the SRAM buffer is mapped by the base address of the corresponding NAND FCM bank (chip-select) by setting IFC_CSPRn[BA].

You could refer to u-boot definition include/configs/ls1043ardb.h.

#define CONFIG_SYS_NAND_BASE 0x7e800000
#define CONFIG_SYS_NAND_BASE_PHYS CONFIG_SYS_NAND_BASE

#define CONFIG_SYS_NAND_CSPR_EXT (0x0)
#define CONFIG_SYS_NAND_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| CSPR_PORT_SIZE_8 \
| CSPR_MSEL_NAND \
| CSPR_V)
#define CONFIG_SYS_NAND_AMASK IFC_AMASK(64*1024)

 

#define CONFIG_SYS_CSPR1_EXT CONFIG_SYS_NAND_CSPR_EXT
#define CONFIG_SYS_CSPR1 CONFIG_SYS_NAND_CSPR
#define CONFIG_SYS_AMASK1 CONFIG_SYS_NAND_AMASK
#define CONFIG_SYS_CSOR1 CONFIG_SYS_NAND_CSOR

0 项奖励
回复