LS1023/LS1043/LS1012A 100BASE-FX support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1023/LS1043/LS1012A 100BASE-FX support

4,427件の閲覧回数
carlos-m-ribeiro
Contributor I

Hi,

By default, is there support in u-boot of LS1023/LS1043/LS1012A to connecting directly an 100BASE-FX FPGA to SGMII of LS1023/LS1043/LS1012A?

Thank you

 

0 件の賞賛
返信
3 返答(返信)

4,414件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
  •        NXP designs to an attachment unit interface (AUI) specification (MII, GMII, RGMII, SGMII, etc.), so in most cases proper operation is achieved if the interface signal requirements (timings, IO levels, etc.) are met.  This includes PHYless designs as well.
  •        Input Output Buffer Information Specification (IBIS) modeling can help determine signal degradation to/from our device across the interconnect.
  •        Actual medium support (copper, fiber, coax, etc) is dependent on the Medium Attachment Unit (MAU) connected to our device (PHY, Switch, FPGA, etc).

 

So, 100BASE-FX is not an interface supported by our SoCs.

SGMII with 8b/10b encoding is the best we have to offer to get 100Mbps with an optical connection.

Can the FPGA connect to the LS device via SGMII?

 

As a side note, naming conventions can get confusing. We do list a 1000BASE-X mode but this is really just SGMII with the rate-adaptation logic disabled.

0 件の賞賛
返信

4,409件の閲覧回数
carlos-m-ribeiro
Contributor I

Hello,

No, we have on the FPGA side, 100BASE-FX.

Thank you

0 件の賞賛
返信

4,377件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

From the AE team.

I tried to put in a slide deck to summarize the supported interfaces by the various controllers. The FPGA must connect to the MAC via a supported interface.

The slide deck is a work in progress. So, please share any corrections or suggestions.

0 件の賞賛
返信