LS1023/LS1043/LS1012A 100BASE-FX support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1023/LS1043/LS1012A 100BASE-FX support

4,421 Views
carlos-m-ribeiro
Contributor I

Hi,

By default, is there support in u-boot of LS1023/LS1043/LS1012A to connecting directly an 100BASE-FX FPGA to SGMII of LS1023/LS1043/LS1012A?

Thank you

 

0 Kudos
Reply
3 Replies

4,408 Views
yipingwang
NXP TechSupport
NXP TechSupport
  •        NXP designs to an attachment unit interface (AUI) specification (MII, GMII, RGMII, SGMII, etc.), so in most cases proper operation is achieved if the interface signal requirements (timings, IO levels, etc.) are met.  This includes PHYless designs as well.
  •        Input Output Buffer Information Specification (IBIS) modeling can help determine signal degradation to/from our device across the interconnect.
  •        Actual medium support (copper, fiber, coax, etc) is dependent on the Medium Attachment Unit (MAU) connected to our device (PHY, Switch, FPGA, etc).

 

So, 100BASE-FX is not an interface supported by our SoCs.

SGMII with 8b/10b encoding is the best we have to offer to get 100Mbps with an optical connection.

Can the FPGA connect to the LS device via SGMII?

 

As a side note, naming conventions can get confusing. We do list a 1000BASE-X mode but this is really just SGMII with the rate-adaptation logic disabled.

0 Kudos
Reply

4,403 Views
carlos-m-ribeiro
Contributor I

Hello,

No, we have on the FPGA side, 100BASE-FX.

Thank you

0 Kudos
Reply

4,371 Views
yipingwang
NXP TechSupport
NXP TechSupport

From the AE team.

I tried to put in a slide deck to summarize the supported interfaces by the various controllers. The FPGA must connect to the MAC via a supported interface.

The slide deck is a work in progress. So, please share any corrections or suggestions.

0 Kudos
Reply