LS1021a PCIe port error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021a PCIe port error

2,677件の閲覧回数
jiye
Contributor V

Has anyone encountered this error ever before?

I am not able to boot into the rootfs.

Kernel 4.19 Debian distribution

[  172.125566] Internal error: : 1210 [#1] SMP ARM
[  172.126425] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  172.130095] Modules linked in: caam_jr caamhash_desc caamalg_desc ath10k_pci ath10k_core ath mac80211 cfg80211 caam error
[  172.138127] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  172.148996] CPU: 1 PID: 65 Comm: kworker/u4:1 Not tainted 4.19.46-dirty #46
[  172.149000] Hardware name: Freescale LS1021A
[  172.149120] Workqueue: ath10k_wq ath10k_core_register_work [ath10k_core]
[  172.158678] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  172.165584] PC is at ath10k_pci_wake_wait+0x30/0xb0 [ath10k_pci]
[  172.165604] LR is at arch_timer_read_counter_long+0x14/0x18
[  172.169839] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  172.176494] pc : [<bf1ce8a8>]    lr : [<c0233008>]    psr: 800f0093
[  172.176500] sp : eef3be00  ip : 00000000  fp : 000abbe7
[  172.176505] r10: f1106ed4  r9 : eddcbe00  r8 : c0cdfaa4
[  172.176511] r7 : 0000752f  r6 : eddc8e00  r5 : 00000069  r4 : 00000023
[  172.176523] r3 : f0f80000  r2 : 00080000  r1 : 00000000  r0 : 00000176
[  172.184850] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  172.190797] Flags: Nzcv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user
[  172.196358] pcieport 0000:00:00.0: can't find device of ID0000
[  172.203080] Control: 30c5387d  Table: ad9deac0  DAC: bffefcef
[  172.259393] Process kworker/u4:1 (pid: 65, stack limit = 0xe0d1b8d1)
[  172.265732] Stack: (0xeef3be00 to 0xeef3c000)
[  172.270081] be00: eddc8e00 eddccf48 eddcce00 200f0013 f0f80004 00000001 f1106ed4 bf1cedec
[  172.278240] be20: eddc8e00 0003442c eddcbe00 eddcce00 bf1b1ff8 eddc9268 f1106ed4 bf1cef38
[  172.286403] be40: eebc7680 eef3be54 c1006494 eddc8e00 00034400 eddcbe00 00000001 bf19f2a8
[  172.294564] be60: eddc8e00 eddcbe00 eddc99d0 eddc9520 00000000 bf1d037c eddc8e00 bf1d0db0
[  172.302730] be80: eddc8e00 eddc8e00 eddcce00 bf1d03ac eddc8e00 c1006494 ffffff92 bf18137c
[  172.310893] bea0: 00333135 21ab92a6 00000000 eddc8e00 00000000 21ab92a6 00001234 eddc8e00
[  172.319044] bec0: eddc9a88 c1006494 eddc9984 eddc8e08 eddc99bc bf1b2540 00000000 bf183068
[  172.327190] bee0: eddcba88 00000000 00000000 05030000 00000008 21ab92a6 00000000 eddcba88
[  172.335335] bf00: eef18280 ee808400 ee909400 00000000 c10bfe24 00000000 ee808400 c0273ae0
[  172.343481] bf20: ee808400 ee808400 c1003d00 eef18280 ee808400 eef18294 c1003d00 ee808418
[  172.351627] bf40: ffffe000 00000088 ee808400 c02749d4 ffffe000 c10bf605 c0c21d5c 00000000
[  172.359773] bf60: ffffe000 ee8b7b40 eee260c0 00000000 eef3a000 eef18280 c0274990 ee8dbea4
[  172.367920] bf80: ee8b7b5c c0279820 00000001 eee260c0 c02796d4 00000000 00000000 00000000
[  172.376065] bfa0: 00000000 00000000 00000000 c02011f8 00000000 00000000 00000000 00000000
[  172.378533] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[  172.384209] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[  172.384221] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[  172.384278] [<bf1ce8a8>] (ath10k_pci_wake_wait [ath10k_pci]) from [<bf1cedec>] (ath10k_pci_wake.part.4+0x88/0xb0 [ath10k_pci])
[  172.384319] [<bf1cedec>] (ath10k_pci_wake.part.4 [ath10k_pci]) from [<bf1cef38>] (ath10k_bus_pci_read32+0x68/0xb0 [ath10k_pci])
[  172.429198] [<bf1cef38>] (ath10k_bus_pci_read32 [ath10k_pci]) from [<bf19f2a8>] (ath10k_ce_disable_interrupts+0x5c/0x140 [ath10k_core])
[  172.441382] [<bf19f2a8>] (ath10k_ce_disable_interrupts [ath10k_core]) from [<bf1d037c>] (ath10k_pci_irq_disable+0xc/0x20 [ath10k_pci])
[  172.453435] [<bf1d037c>] (ath10k_pci_irq_disable [ath10k_pci]) from [<bf1d0db0>] (ath10k_pci_warm_reset+0x34/0x204 [ath10k_pci])
[  172.464968] [<bf1d0db0>] (ath10k_pci_warm_reset [ath10k_pci]) from [<bf1d03ac>] (ath10k_pci_hif_stop+0x1c/0xc0 [ath10k_pci])
[  172.476194] [<bf1d03ac>] (ath10k_pci_hif_stop [ath10k_pci]) from [<bf18137c>] (ath10k_core_start+0x6a0/0xaf0 [ath10k_core])
[  172.487370] [<bf18137c>] (ath10k_core_start [ath10k_core]) from [<bf183068>] (ath10k_core_register_work+0x5dc/0x894 [ath10k_core])
[  172.499110] [<bf183068>] (ath10k_core_register_work [ath10k_core]) from [<c0273ae0>] (process_one_work+0x218/0x50c)
[  172.509505] [<c0273ae0>] (process_one_work) from [<c02749d4>] (worker_thread+0x44/0x5bc)
[  172.517567] [<c02749d4>] (worker_thread) from [<c0279820>] (kthread+0x14c/0x154)
[  172.524936] [<c0279820>] (kthread) from [<c02011f8>] (ret_from_fork+0x14/0x3c)
[  172.532122] Exception stack(0xeef3bfb0 to 0xeef3bff8)
[  172.537151] bfa0:                                     00000000 00000000 00000000 00000000
[  172.545294] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[  172.553434] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[  172.560024] Code: e596223c e5993e34 e5922058 e0833002 (e5933000)
[  172.566091] ---[ end trace 50029c4263d891e3 ]---
[  172.595366] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[  172.601790] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  172.609914] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  172.619515] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  172.627875] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[FAILED] Failed to start Network Manager Wait Online.
See 'systemctl status NetworkManager-wait-online.service' for details.
[  172.688797] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready
[  172.719732] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready
[  173.400720] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  173.408816] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  173.418419] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  173.426788] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  173.433597] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  173.441608] pcieport 0000:00:00.0: can't find device of ID0000

Debian GNU/Linux 9 localhost ttyS0

localhost login: [  173.841968] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  173.850002] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  173.859826] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  173.868163] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  173.874940] pcieport 0000:00:00.0:    [ 8] Rollover              
[  173.881018] pcieport 0000:00:00.0:    [12] Timeout               
[  173.887113] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  173.895104] pcieport 0000:00:00.0: can't find device of ID0000
[  173.900907] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  173.908889] pcieport 0000:00:00.0: can't find device of ID0000
[  175.688426] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  175.696471] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  175.706029] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  175.714399] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  175.768492] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  175.776512] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  175.786343] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  175.794672] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  175.801426] pcieport 0000:00:00.0:    [ 8] Rollover              
[  175.807516] pcieport 0000:00:00.0:    [12] Timeout               
[  175.813584] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  175.821573] pcieport 0000:00:00.0: can't find device of ID0000
[  175.827392] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  175.835377] pcieport 0000:00:00.0: can't find device of ID0000
[  175.968999] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  175.977027] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  175.986586] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  175.994947] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  176.137935] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.145958] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  176.155528] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  176.163860] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  176.380504] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.388530] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  176.398348] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  176.406709] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  176.413470] pcieport 0000:00:00.0:    [ 8] Rollover              
[  176.419569] pcieport 0000:00:00.0:    [12] Timeout               
[  176.425685] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.433661] pcieport 0000:00:00.0: can't find device of ID0000
[  176.545109] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.553094] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  176.562940] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  176.571303] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  176.578108] pcieport 0000:00:00.0:    [ 8] Rollover              
[  176.584210] pcieport 0000:00:00.0:    [12] Timeout               
[  176.590289] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.598299] pcieport 0000:00:00.0: can't find device of ID0000
[  176.604160] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.612134] pcieport 0000:00:00.0: can't find device of ID0000
[  176.732811] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.740837] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  176.750417] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  176.758771] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  176.765595] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.773573] pcieport 0000:00:00.0: can't find device of ID0000
[  176.791855] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  176.799851] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  176.809392] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  176.817719] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  177.518169] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  177.526201] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  177.535764] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  177.544128] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  178.459919] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  178.467959] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  178.477539] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  178.485916] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  179.139845] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.147866] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  179.157709] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  179.166072] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  179.172850] pcieport 0000:00:00.0:    [ 8] Rollover              
[  179.178952] pcieport 0000:00:00.0:    [12] Timeout               
[  179.185074] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.193052] pcieport 0000:00:00.0: can't find device of ID0000
[  179.198911] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.206920] pcieport 0000:00:00.0: can't find device of ID0000
[  179.569402] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.577430] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  179.587008] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  179.595368] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  179.602154] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.610167] pcieport 0000:00:00.0: can't find device of ID0000
[  179.753071] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.761097] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  179.770655] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  179.779005] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  179.909300] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  179.917322] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  179.926892] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  179.935237] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  180.597786] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  180.605838] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  180.615675] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  180.624051] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  180.630832] pcieport 0000:00:00.0:    [ 8] Rollover              
[  180.636939] pcieport 0000:00:00.0:    [12] Timeout               
[  180.643033] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  180.651047] pcieport 0000:00:00.0: can't find device of ID0000
[  180.910098] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  180.918115] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  180.927674] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  180.936007] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  181.074822] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  181.082807] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  181.092386] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00000001/00006000
[  181.100752] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  181.107571] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  181.115600] pcieport 0000:00:00.0: can't find device of ID0000
[  181.138142] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  181.146165] pcieport 0000:00:00.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Transmitter ID)
[  181.156008] pcieport 0000:00:00.0:   device [1957:0e0a] error status/mask=00001101/00006000
[  181.164348] pcieport 0000:00:00.0:    [ 0] RxErr                  (First)
[  181.171098] pcieport 0000:00:00.0:    [ 8] Rollover              
[  181.177177] pcieport 0000:00:00.0:    [12] Timeout               
[  181.183247] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  181.191235] pcieport 0000:00:00.0: can't find device of ID0000
[  181.197057] pcieport 0000:00:00.0: AER: Multiple Corrected error received: 0000:00:00.0
[  181.205041] pcieport 0000:00:00.0: can't find device of ID0000

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,513件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which board and PCIe module are used?

Please provide description (or block diagram) of the system in question.

0 件の賞賛
返信

2,513件の閲覧回数
jiye
Contributor V

I just re flashed the device to fix the error thanks for the reply

0 件の賞賛
返信