LS1021A - RGMII eTSEC3, no 125MHz on EC3_GTX_CLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A - RGMII eTSEC3, no 125MHz on EC3_GTX_CLK

2,228件の閲覧回数
Davisg
Contributor III

I have an LS1021A board designed by our customer that is configured for RGMII eTSEC3 using the same PHY (AR8033) as LS1021A-TWR board and connected exactly the same as the LS1021A-TWR board. Good 1Gbps link on Ethernet port. U-boot reports "Speed: 1000, full duplex" but fails ping with "not alive".

On LS1021A-TWR observe 125MHz clock on EC3_GTX_CLK when transmitting (ping from u-boot with "alive").

On LS1021A board (not tower) there is no 125MHz clock on EC3_GTX_CLK when trying to transmit (ping from u-boot). There is activity on the EC3_GTX_CLK signal but it does not look like a clock (i.e., not 125MHz, 25MHz, or 2.5MHz clock).

I have not been able to find what is causing this yet.

ラベル(1)
0 件の賞賛
返信
1 返信

2,022件の閲覧回数
Davisg
Contributor III

Problem was found to be improper termination on EC3_GTX_CLK125 clock source

0 件の賞賛
返信