LS1021A PCIe Wifi Interface Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A PCIe Wifi Interface Issue

1,498 Views
jiye
Contributor V

Anyone knows what's the issue here.

My kernel does have the interface up

But after I scan there are no wifi names showing up

pastedImage_1.png

pastedImage_1.png

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,405 Views
bpe
NXP Employee
NXP Employee

This is a  device-specific problem, which, based on the provided screen
captures, is a result of device's failure to respond to certain commands.
This is totally the driver and underlying HW specific, thus the suggestion
is to approach your radio card manufacturer for more detailed error output
interpretation and troubleshooting.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply