LS1021A Device mode (g_ether)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A Device mode (g_ether)

1,595件の閲覧回数
jiye
Contributor V

I have a stand alone ls1021a device and my schematic is like this below:

pastedImage_1.png

My PC can't detect my ls1021a device over USB3.0 I want to configure it as OTG g_ether device.

I want to ask couple things here:

(1) for device mode is the USB1_ID should be floating or pull up

(2) do I need to add pull down resistors at USB1_D_M and USB1_D_P

(3) what else do I have to fulfill?

(4)

pastedImage_1.png

Is USB g_ether OTG is a A device or B device in the picture above?

ラベル(1)
0 件の賞賛
返信
1 返信

1,534件の閲覧回数
Pavel
NXP Employee
NXP Employee

(1) USB1_ID should be floating for device mode. See the following Application Note:

https://www.maximintegrated.com/en/design/technical-documents/tutorials/1/1822.html

 

(2) External resistors are not needed for the LS1021a USB1.  The LS1021a USB1 includes USB PHY. This PHY uses internal resistors.

 

(3) Use as example for USB using the TWR-LS1021a board schematic:

https://www.nxp.com/webapp/Download?colCode=TWR-LS1021A-PB-DF&location=null

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信