LS1021A: Bypass RCW electrically

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A: Bypass RCW electrically

1,741件の閲覧回数
z_v
Contributor I

Hello,

In the TWR, SW-2\3 are used also to bypass the burned RCW. 

How ? What bits in the RCW can be bypassed this way ?

Thank you,

Z.V

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,604件の閲覧回数
ufedor
NXP Employee
NXP Employee

> In the TWR, SW-2\3 are used also to bypass the burned RCW. 

Sorry, in which document this is stated?

0 件の賞賛
返信

1,604件の閲覧回数
z_v
Contributor I

Hi Ufedor,

For example:

S3.5 : 0 - NOR bank 0 

          1 -  NOR bank 1

How does S3.5 affects the source from where u-boot runs ?

Who reads the position of the switches ?

Thank you,

Z.V

0 件の賞賛
返信

1,604件の閲覧回数
ufedor
NXP Employee
NXP Employee

S3.5 is connected to the CPLD which controls MSb of the NOR Flash address.

0 件の賞賛
返信