LS1021A: Bypass RCW electrically

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A: Bypass RCW electrically

1,733 次查看
z_v
Contributor I

Hello,

In the TWR, SW-2\3 are used also to bypass the burned RCW. 

How ? What bits in the RCW can be bypassed this way ?

Thank you,

Z.V

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,596 次查看
ufedor
NXP Employee
NXP Employee

> In the TWR, SW-2\3 are used also to bypass the burned RCW. 

Sorry, in which document this is stated?

0 项奖励
回复

1,596 次查看
z_v
Contributor I

Hi Ufedor,

For example:

S3.5 : 0 - NOR bank 0 

          1 -  NOR bank 1

How does S3.5 affects the source from where u-boot runs ?

Who reads the position of the switches ?

Thank you,

Z.V

0 项奖励
回复

1,596 次查看
ufedor
NXP Employee
NXP Employee

S3.5 is connected to the CPLD which controls MSb of the NOR Flash address.

0 项奖励
回复