LS1021: Use multiple Hard drives on the SATA port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021: Use multiple Hard drives on the SATA port

Jump to solution
1,736 Views
Sebster
Contributor II

Hello,

I would like to know if the LS1021 single SATA controller can control more than one Hard drive? The idea is to connect two Hard drives on two different Serdes Lanes (Pairs) and have the SATA controller flip flop between the two Hard drives as needed. Is the SATA controller intelligent enough to do this Automatically?

Thanks for your help, much appreciated

SPA

Labels (1)
0 Kudos
Reply
1 Solution
1,592 Views
ufedor
NXP Employee
NXP Employee

Described approach is not viable.

The LS1021A SATA controller supports port multiplier operation, so it is possible to use an external port multiplier device.

View solution in original post

0 Kudos
Reply
2 Replies
1,592 Views
Sebster
Contributor II

Hi Fedor,

Thanks for the answer.
Seb

0 Kudos
Reply
1,593 Views
ufedor
NXP Employee
NXP Employee

Described approach is not viable.

The LS1021A SATA controller supports port multiplier operation, so it is possible to use an external port multiplier device.

0 Kudos
Reply