LA1028A EEPROM problem consultation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LA1028A EEPROM problem consultation

2,122件の閲覧回数
jack_huang1
Contributor IV

In the LS1028A schematic, there are three different EEPROM devices, what are the functions respectively? Is there a detailed documentation? In the design, can it be removed? Thank you very much!微信图片_20220220122001.png

0 件の賞賛
返信
1 返信

2,116件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1028A Reference Design Board Reference Manual, Table 15. I2C1 bus device map.

> In the design, can it be removed?

U47 can be removed if booting from I2C is not needed.

U50 can be removed if hard-coded DDR controller settings are provided in the TF-A BL2.

0 件の賞賛
返信